- Published 23 Apr 2023
- Last Modified 29 Aug 2023
- 5 min
How Do Gas Detectors Work?
Discover how both domestic and industrial gas detectors protect you and those around you from hazardous fumes.
![](http://res.cloudinary.com/rspoc/image/upload/w_1248,h_180,c_crop,c_fill,f_auto,q_auto/dpr_auto/v1675961765/RS%20CONTENTFUL/Discovery/Hero%20Banners/Gas%20Detectors/9_SEO_Gas_Detectors_5120x360px.jpg)
Both at home and at work, gas detectors help keep us safe. As well as being a legal requirement in some environments, they’re installed to protect against the potentially fatal effects of gases like carbon monoxide, natural gas, methane, and ammonia.
Gas detectors work by measuring the amount of a certain gas in the surrounding air and sending an alert when the concentration level of this substance gets too high. Depending on the specific type of gas, each detecting device will work slightly differently.
This guide will explain exactly how gas detectors work, outline how they’re calibrated, and give advice on finding the right one for your needs.
Gas Detection Equipment
Getting the right gas detection equipment relies on knowing which gas you want to detect and the environment you need to protect. For example, gas leak detectors help to find the source of released fumes while gas analysers or gas meters give readings of a specific substance in the surrounding atmosphere.
Alongside choosing the right type of gas detector, having accessories such as mounting sockets, probes, and cases will help improve the accuracy of each measurement. Calibrating the sensor of choice regularly, ideally every six to twelve months, according to the manufacturer’s instructions, will also ensure your detector is truly keeping people safe.
How Many Types of Gas Detectors are there?
Every type of detector or analyser is designed to measure particular types of gas, be they domestic or industrial gas detectors. This means they have different types of sensors. The main types of gas-detecting sensors are:
- Catalytic: these use a catalytic wire made from elements that oxidise in the presence of combustible gases in the atmosphere alongside a wire that doesn’t. As the one wire oxidises, resistance in it increases. The difference between the resistance of the two wires triggers a response in the detector's circuit and raises the alarm
- Infrared: these types of detectors have a light transmitter and receiver. When combustible gases pass between the transmitter and receiver, it changes the nature of the light. This change is picked up by the receiver and an alarm is triggered
- Electrochemical: these use electrodes to detect toxic gases in the air. When certain gases come into contact with the sensor electrodes, a chemical reaction occurs and triggers the flow of electrons. The current this generates is measured and a level of gas in the air is given on the detector
- Metal oxide semiconductors: otherwise known as MOS detectors, they contain a film that has electrons flowing freely through it when heated. In the presence of oxygen, this flow is restricted. Yet when the level of another gas is high, the flow is increased, as is the resistance in the detector, triggering an alarm
Depending on the specific type of gas you’re trying to detect and the particular environment you’re measuring it in, different gas detectors will be appropriate.
Carbon Monoxide Detectors
High levels of carbon monoxide are toxic and can cause real damage to health if an individual is exposed for an extended period of time. Having a carbon monoxide alarm in a house or working environment will help detect any leaks from generators, grills, or heating systems. Most carbon monoxide detectors work using electrochemical or MOS sensors.
Natural Gas Detectors
Natural gas can’t be seen and often won’t be smelt until it's in a high concentration. However, it poses a safety threat due to its high combustibility. Available as handheld and fixed sensors, natural gas detectors often use infrared or catalytic systems to alert people to the presence of this substance. Catalytic systems have been used as industrial gas detectors in coal mines since 1959.
Ammonia Gas Detectors
Most often present in factories, warehouses, and other commercial environments, ammonia has a strong smell but is colourless and can quickly become a danger to health if a leak occurs. Irritating to the eyes, nose and throat, it can cause coughing, internal damage, and be fatal after 30 minutes of exposure. Using handheld MOS and electrochemical sensors or probes can give early warning signs to minimise the risk.
Methane Gas Detectors
Industrial gas detector solutions are required in environments such as chemical plants and agriculture. Some manufacturing processes will also handle products or use processes that make high levels of methane. If there’s a high concentration of methane in the air, it can risk potential explosions and fire hazards. Catalytic and infrared gas detectors will sound the alarm when large amounts of methane are in the air, helping to keep teams safe at work.
Do Carbon Monoxide Detectors Detect Natural Gas?
Carbon monoxide and natural gas risk safety in two different ways. When inhaled, carbon monoxide damages red blood cells and stops the natural flow of oxygen around the body and organs. After extended exposure, this can start to cause symptoms such as headaches and nausea and even lead to death.
In contrast, natural gas is highly flammable and can cause explosions or fire hazards when present in high concentrations. For these reasons, both gases are a danger in homes and commercial environments and can’t be detected by the same sensors.
Electrochemical and MOS sensors are best for detecting carbon monoxide as this gas triggers chemical reactions in the detectors. Meanwhile, catalytic and infrared sensors detect an increase in levels of natural gas by monitoring the movement of air. This means carbon monoxide detectors won’t be triggered by an increase in levels of natural gas.